4/5/2019 1:04 PM | |
Posts: 16 Rating: (1) |
Dear all, i have used S7 1200 214-1AG40-0XB0 is it possible to configure output as a NPN ? if yes then please revert. |
Last edited by: Pavy at: 4/5/2019 1:05:07 PM |
|
4/5/2019 2:18 PM | |
Posts: 2826 Rating: (685) |
Hello. You have one of three options: 1. Build an external electronic interface circuit. Search the web for suggestions. 2. Study the manual of the stepper driver. Most models mention how PNP connections can be made. Be on the look out when is 24V or 5V needed. 3. Use a signal board on the S7-1200. The wiring diagram is attached; special focus on the text below the diagram. BR Attachmentabout-signal-board.pdf (500 Downloads) |
4/10/2019 9:02 AM | |
Posts: 16 Rating: (1) |
Thank u so much for given your valuable time. |
Follow us on