4/4/2016 9:56 AM | |
Joined: 4/24/2006 Last visit: 9/18/2024 Posts: 8738 Rating: (1168) |
Hello, Do I understand it right: The output is not switching, but in Program iit is 'green'? Best regards, Wizard |
4/5/2016 10:51 AM | |
Posts: 146 Rating: (0) |
I think ...you should download hardware (in overview config device) for your expansion module ..then ..you working with them ! |
5/1/2016 7:00 PM |
|
Posts: 198 Rating: (36) |
I think your hardware configuration is missing first add all expansion module through hardware catalog right side of the program. I think you just add one cpu only .any way you make a mistake because this is your first project . read this book TIA Portal includes STEP 7 for S7-1200 programming
|
8/9/2017 11:32 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by Farzad_Sadr is split to a separate thread with the subject When connect power to the digital input, nothing happens - The corresponding LED lights up but nothing on the output side.. Best regards |
Follow us on