6/4/2017 10:12 PM | |
Joined: 1/24/2008 Last visit: 12/4/2019 Posts: 41 Rating:
|
Dear Members I want to use S7 1200 series PLC for a project having more I/Os than the CPU series can handle. Could you suggest me a combination using S7 1200 CPUs in Master/Slave mode? A sample project or an illustration would be highly appreciated ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/9/2017 3:35:31 PMNew subject after splitting |
|
6/12/2017 9:42 AM | |
Joined: 5/15/2010 Last visit: 12/8/2019 Posts: 168 Rating:
|
IO device is refereed here as interface modules? |
Regards |
|
6/12/2017 11:46 AM | |||||||
Joined: 3/5/2014 Last visit: 12/13/2019 Posts: 3859 Rating:
|
hi, yes, S7-1200 CPUs have an addressarea of 1kbyte which is completely in the process-image. An overview of the S7-1200 models you find in the s7-1200 system-manual, chapter 1: SIMATIC S7 S7-1200 Programmable controller hope this helps, regards, |
||||||
There is no bad feedback! |
|||||||
6/13/2017 6:08 AM | |
Joined: 5/15/2010 Last visit: 12/8/2019 Posts: 168 Rating:
|
i have a confusion, please let me know if i am wrong or right. I have read the manual, process image area for input and output is 1kbyte i.e. 1024 Bytes. Does this means the CPU can have 1028/8=128 digital and 1024/8=128 digital output cards. Or We can define from 0-128 as input and output address. |
Regards |
|
Follow us on