5/26/2016 4:46 PM | |
Posts: 24 Rating: (0) |
Hi, i want to use the plc web server to log data. i set the ip address for plc to 192.168.0.1, and i open the browser with http://192,168.0.1, but it said, this page can not be displayed. So is there anything wrong with my setting? Wating for help. And the hardware is S7-1200, the software is TIA portal. Thanks a lot. |
5/26/2016 4:59 PM | |
Posts: 24 Rating: (0) |
By the way, i have enabled ''activate webserver on this module''. |
5/27/2016 9:11 AM | |
Posts: 24 Rating: (0) |
now i successfully enter the website, but there is only the start page. Could anyone tell me why? |
5/27/2016 2:22 PM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22230 Rating: (2980) |
what want you more? |
5/27/2016 4:12 PM | |
Posts: 24 Rating: (0) |
Ok, i see. i need to use the www Funktion. |
5/28/2016 11:38 AM | |
Joined: 5/29/2013 Last visit: 4/19/2024 Posts: 100 Rating: (28) |
In the hardware configuration (where you enabled the webserver) you also need to set a user and password with for example Admin rights. Also the default could be set as administrator so everyone could do everything. when you use them in the start page a lot of options and pages become available. also you log files and a link to your user page. for more information about using the webpage and even make it dynamic using Javascript DMC made a good helpfull page that will get you started. DMC S7-1200 webserver and javascript |
Regards |
|
7/21/2016 2:52 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by AutoGen_4329155 is split to a separate thread with the subject webserver with a 1212C CPU, old date in diagnostic buffer. Best regards |
Follow us on