Industry Online Support
Technical Forum
11/25/2014 8:37 AM | |
Posts: 8 Rating: (1) |
Hello. Have a problem with maximum records for .csv log file. Here explained that for s7-1214 is 500kB limit for one log file. When I set 4700 records in DataLogCreate instruction it allows to create log file (it's size 280kB). But if I set 4800 records or more it doesn't allow me to log. DataLogCreate instruction doesn't react on positive signal edge at all (status is 16#7000). With 4700 records file created there still 90% free space on load memory. Any ideas how to increase amount of records to maximum allowed? -------------------- New subject after splitting from Sample program: S7-1200 and DATA LOG |
Last edited by: Min_Moderator at: 11/25/2014 3:52 PMSplitted Last edited by: Igor_B at: 11/25/2014 10:07 AM |
|
11/28/2014 4:22 PM | |
Posts: 267 Rating: (22) |
Hello, you can build a sequencer that decrease the RECORDS from 4800 and stop if you get a positive STATUS. |
12/3/2014 4:06 PM | |
Joined: 7/7/2010 Last visit: 5/13/2024 Posts: 14710 Rating: (2359)
|
When you need to know "why" there are limits, this is the place to start: Support Request When you find answers, please post back here! |
science guy |
|
12/5/2014 3:14 PM | |
Posts: 8 Rating: (1) |
As technical support told me It's known problem. Regardless this information about limits of .csv log files sizes still for firmware V3.x in internal memory you can create max 375kB file. This changed in V4.x. |
This contribution was helpful to2 thankful Users |
Follow us on