12/21/2012 1:32 AM | |
Posts: 12 Rating:
|
Anyone please advice, why i cannot surf to the S7-1214C webserverlogin pages. I'm currently using S7-1214CAC/DC CPU, with FW v2.2.I did enable the webserver and write protectionoption via TIA V11,S7-1214C IP was 192.168.0.1 and my laptop IP192.168.0.88, subnet 255.255.255.0.Withthis congfiguration i tired to connect the PLC andLaptop with ethernet cable and inserthttp://192.168.0.1 to the internet explorer 8.but is still cannot surf to the main log in pages. Can anyone here please advice what do i miss in the congfiguration ? Thanks. |
12/22/2012 1:39 AM | |
Posts: 12 Rating:
|
Hi Huggy, The laptop is able to ping with the PLC and I'm currently using IE8. it will ask for certificate when only i key in https://zz.xx.ww.cc but when im using http://zz.xx.ww.cc it just display unable to connect. do you have any idea what is the problem ? |
12/26/2012 3:21 AM | |
Posts: 12 Rating:
|
Can anyone help please ? |
12/26/2012 4:04 PM | |
Joined: 11/27/2012 Last visit: 8/6/2019 Posts: 17 Rating:
|
i think you must connect to your plc with other computer and erase plc memori and after you can try |
1/2/2013 4:23 PM | |
Joined: 7/7/2010 Last visit: 3/5/2021 Posts: 10212 Rating:
|
Do you have the web server only allow secure connections configured? {Checkbox below web server enable, "Permit access only with https"} If so, then the http://192.168.0.1 link will not work. |
science guy |
|
Follow us on