9/1/2019 11:08 PM | |
Joined: 9/1/2019 Last visit: 9/8/2019 Posts: 1 Rating:
|
Dear Denilson, I was reviewing the S7 1500 PLC manuals, but I could not find a Modbus TCP communication module. The Modbus TCP can be used through the integrated CPU processor, but this is done through the profinet link. Is there a dedicated module of communication with Modbus TCP protocol? to place it as an input and / or output module that this module is independent of the CPU. Regards, Favio ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/02/2019 07:14:08New subject after splitting |
|
Follow us on