(0)| 11/26/2018 2:23 AM | |
|
Posts: 2 Rating:
|
Hi everyone, I need to send ASCII commands to an electronic balance (for example : "TARE", "PRINT"). The balance reference is Shimadzu UX4200: Communication protocol of the balance is RS232. CPU is S7 1517F-3 PN/DP and only Profinet port is available. GSD file is provided by the gateway manufacturer and installed. After having looked for documentation, I think I have to use acyclic communication because commands to the balance must be sent when the user decides it. So using SFB52 and SFB53 (RDREC and WRREC) should do the trick, right? Any help or tips would be welcome. edit:title |
Last edited by: nicolas_ at: 11/29/2018 3:01:48 AM |
|
| 11/26/2018 8:15 AM | |
|
Joined: 12/13/2011 Last visit: 10/1/2024 Posts: 146 Rating:
|
hello I pass a project that I did, as much as the hadware as the fc and db. AttachmentPictures.zip (277 Downloads) |
This contribution was helpful to
|
|
Follow us on