Industry Online Support
Technical Forum
4/29/2011 12:04 AM | |
Posts: 34 Rating: (0) |
Hi guys, I am traying to communicate S7-200 with winccflexible2008SP2 pc runtime on windows 7(error is same for windows xp) using USB/PPI adapter.But when i try to communicate it gives connection disconnected error code 41001 and also general error 0xce.However i can access Plc through microwin on same computer.I also made all PG/PC seeting according to following manual http://support.automation.siemens.com/WW/view/en/28263099 But still the problem is same.....plz reply urgently Thanks |
Last edited by: O_Moderator at: 4/29/2011 7:39 AMlink edited |
|
5/1/2011 9:02 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, The same issue like in that thread - establish communication between WinCC flexible and STEP 7-Micro .. Unfortunately without any suggestion. Try with reinstalling of software. Best regards, Hristo Mihalev |