5/20/2011 4:49 PM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Hello, Are you sure that with wipeout.exe wasn't helpful? I mean do you use the cable before to connect to other CPU? What are the settings in PG/PC Interface? When the RUN light is ON do you have some outputs active there? best regards, Hristo Mihalev |
5/21/2011 7:53 AM | |
Posts: 4 Rating: (0) |
Hi, Yes I try wipeout and I can't connect.I can connect with this cable and PC the others S7-200 CPUs. I attach a picture about PG/PC interface and S7-200 CPU picture.I try 24VDC to DI of CPU But The CPU don't response and don't light the led of the DI.Maybe İt lock the CPU. AttachmentS7-200.zip (625 Downloads) |
5/22/2011 7:28 AM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Maybe is better to contact with Siemens (Support Request). Could be, in case of new CPU - to be deffective. Best regards, Hristo Mihalev |
9/8/2011 4:44 AM | |
Posts: 11 Rating: (0) |
Hi, All I faced the same problem, I tried to use wipeout.exe but affter followed the instruction , I still got a message "ERROR: Could not connect to CPU! "
|
9/8/2011 9:14 AM | |
Posts: 11 Rating: (0) |
Hi, all My PLC model is S7-200CN AC/DC/RYL ( 6ES7 212-1BB23-0XB8 ) and cable is RS232/PPI Multi-Master Cable (6ES7 901-3CB30-0XA0) actually, I've got USB/PPI too. Problem as shown in Fig01.jpg (SF/DIAG=RED, RUN=GREEN) can not connect to CPU via USB/PPI or RS232/PPI on Step7MicroWin SP7 It's not because of "Language" trouble beacuse another one of my CPU S7-200CN is connected also upload and download. So, I use wipeout.exe but it seem doesn't work as shown in wipeout1.jpg then I connected my CPU to module EM277 PROFIBUS DP as in Fig02.jpg and I tried wipeout.exe again, it's done well as shown in wipeout2.jpg but problem not solvedSF/DIAG=RED, RUN=GREEN and not connect. Thank you.
Attachmentsf_diag.zip (617 Downloads) |
9/8/2011 9:25 AM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Hello, After successfully "cleared" of CPU, can you connect using PPI cables to the CPU? Best regards, Hristo MIhalev |
9/8/2011 1:10 PM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Replace the CPU. Try with support request. |
6/4/2013 1:46 AM | |
Joined: 3/9/2013 Last visit: 6/27/2023 Posts: 1 Rating: (0) |
Hi, |
6/4/2013 7:32 AM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711)
|
Hello, If you have done all steps that are written in this thread, you have a faulty CPU. Here they are again: Test PPI cable with other PLC. Set PLC in Stop with switch. Select search all baudrates. Local adres should not be 2,try different adresses. Disconnect extention modules. Try Wipeout Regards, Marcjan |
Problem solved? |
|
5/7/2014 2:06 PM | |
Posts: 1 Rating: (0) |
i am having a similar issue with a S7-200 plc.It is showing RED LED at SF/DIAG and YELLOW at STOP. Why is this happening and what should i do to rectify this. |
Follow us on