Industry Online Support
Technical Forum
8/4/2009 8:04 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, You have 2 possibilities: For an HMI device connected to the communications port of the S7-200 CPU, with no other devices on the network, select either the PPI or the MPI protocol for the HMI device. Like example you can use Program to set the time of an S7-200 CPU via TP070 and How do you synchronize date/time between a TP170A / TP170micro / TP177micro and an S7-200 CPU with WinCC flexible? Hope this will helps. Best regards, Hristo Mihalev |
Follow us on