7/22/2017 4:31 AM | |
Joined: 7/22/2017 Last visit: 10/26/2022 Posts: 1 Rating: (0) |
Good day! I am new in this forum. I would like to install the softwares needed for Siemens S7 200 (Programmer/HMI and etc). My laptop's currently using Window 7 as its operating system. I've read here and it says that STEP 7-Micro/WIN V4.0.9.25 is compatible for Windows 7 32/64 bit. Where could I find the installer for the specific version of MicroWin? I've asked someone regarding the issue and he said that I should install virtual box to create a virtual operating system and install a windows xp there in order to run the MicroWin application. Which of the two is easier to do? Kindly help me. Thanks! Gab |
7/25/2017 4:54 AM | |
Joined: 7/30/2012 Last visit: 9/16/2024 Posts: 335 Rating: (12) |
Hello Check This Link Hope It Will Help You For Download And Installation... |