11/11/2009 1:39 PM | |
Posts: 62 Rating: (0) |
Hello Experts, I have a project running on a S7200 PLC which has a high speed counter connecting to inputs I0.0 and I0.1. I suspect that the input are bad and would like to connect the counter to two different inputs. when i do this i would now like to change the address in the program so that the high speed counter would see the value coming in. I am not sure how or way the inputs are assigned and would like some help please.i have attached the program also. thanks in advance. Regards, Attachmentramkals perlin machine1.1.zip (533 Downloads) |
11/11/2009 2:19 PM | |
Joined: 4/24/2006 Last visit: 9/18/2024 Posts: 8738 Rating: (1168) |
Dear Raymondk, Here is a link to manual: http://support.automation.siemens.com/WW/view/en/1109582 Please have a look at Chapter 6 (page 118) high speed instructions. It depends on CPU, which HSC are possible. Every HSC has it own input addresses,(see table 6-26) So when you want to use other input addresses, you will have to change High Speed Counter Best regards, Wizard |
11/11/2009 9:20 PM | |
Posts: 62 Rating: (0) |
thank you very much. I will have a look and try this. Thanks, Raymond. |
8/11/2014 11:52 AM | |
Joined: 9/1/2005 Last visit: 9/18/2024 Posts: 4104 Rating: (195) |
new question published by Mechtris split to a seperate thread with the subject add some high Speed inputs - all 6 high Speed counter allready used. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on