3/3/2016 12:30 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (818) |
Hello, didn't work with Smart PLC, but look at this topic: CPU 226 - Not able to communicate with Port 1 (Port 0 is OK) There is project from mr. Jafari, where you can find system of communication, not via RCV but via Interrupt. If you look at help to XMT and RCV instructions, there is also example how set SMB130 to your needs. If you then post some your code, I can probably help you farther. Update: yes, you can use XMT/RCV instructions, or RCV via interrupt (mr. Jafari's prj). |
Last edited by: Duris_I at: 3/3/2016 12:32:36 PMLast edited by: Duris_I at: 3/3/2016 12:33:49 PMWith best regards... |
|
Follow us on