4/23/2016 7:47 AM | |
Joined: 1/21/2016 Last visit: 4/24/2024 Posts: 43 Rating: (8) |
Hello Pratts23, I think you didn't get me. I dont have to open my program in step 7 i just have to change my CPU. So I am asking that is there any special thing i have to take care or any special point that i have to look after for changing it for same philosophy ? Yes ANKURGAMIT i have to see the philosophy but is it possible to change or i have to see some more expects. thankyou for quick reply. |
4/23/2016 8:00 AM | |
Joined: 10/2/2013 Last visit: 4/15/2024 Posts: 339 Rating: (52) |
ET-200 is newer then s7 200 so i think you can do every think which you can do with s7 200 but you have to little study work for high speed input, analog input /output,communication protocol modbus etc if you are using in s7 200. |
Technology is best when it brings people together,so we are here now :) |
|
This contribution was helpful to2 thankful Users |
4/23/2016 9:33 AM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835)
|
The tool was integrated in TIA V10.5 and V11. I don't know why Siemens removed all links for this tool. But if you contacted your local Siemens office, you can get it. Here's some manuals and slides. http://automatizace.hw.cz/files/redaktor6/files/s71200_converter.pdf |
Ayman Elotaify |
|
4/23/2016 11:40 AM | |
Joined: 10/2/2013 Last visit: 4/15/2024 Posts: 339 Rating: (52) |
sir, you mean we have to do it manually with use of v13? if v11 not installed. |
Last edited by: ANKURGAMIT at: 4/23/2016 11:41:59 AMTechnology is best when it brings people together,so we are here now :) |
|
This contribution was helpful to1 thankful Users |
Follow us on