5/16/2006 5:41 PM | |
Posts: 11 Rating: (0) |
Thank you Wizard, |
7/24/2006 5:03 PM | |
Posts: 48 Rating: (4) |
Hello, Please check the following FAQ: http://support.automation.siemens.com/WW/view/en/14188898 It shows the maximum amount of panels that can be connected to one S7-200. As you can see you can connect several panels to one S7-200, also via PPI. Please make sure you use advanced PPI. Originally PPI was a point to point protocol, but the protocol has been adapted and is now capable of multiple master communication. Please make sur ethat DIP switch 5 is switched to multiple master PPI and please make sure to check the advanced PPI option in the PG/PC interface. I hope this information is helpful. Please let me know if the problem has been solved. |