11/15/2015 2:56 PM | |
Posts: 11 Rating: (0) |
Even when I remove the memory, all the lights remain as shown. Including when I use the MEMR. I have not been able to connect via MPI using S7 Lite. |
11/16/2015 3:00 PM | |
Posts: 11 Rating: (0) |
Because I am unable to create an MPI connection to the CPU, I can not change the program on the memory card. |
11/16/2015 3:04 PM | |
Posts: 11 Rating: (0) |
Yes, when I power the unit up and/or hold the MRES switch, no lights change at all. They all stay on solid (as in the image). Not looking good for the CPU :( |
11/16/2015 3:05 PM | |
Posts: 11 Rating: (0) |
With the memory card in or out, the lights just stay as they are. Could it be that I now have two bad CPU's ? |
Follow us on