1/4/2011 8:37 AM | |
Joined: 10/3/2008 Last visit: 4/15/2021 Posts: 853 Rating:
|
Hi, do you mean ModbusTCP or ModbusRTU? Wüstenräuber |
This contribution was helpful to
1 thankful Users |
1/4/2011 9:04 AM | |
Joined: 10/7/2005 Last visit: 4/16/2021 Posts: 2875 Rating:
|
Hello Abdulla the short answer is YES, Siemens does support Modbus, and it supports Modbus RTU as well as Modbus on TCP/IP and it can be a Modbus Master ora ModbusSlave and below are few further links which have all the required details in them. CPU-CPU communication with SIMATIC controllers (compendium)(see chapter 44 & 45) SIMATIC S7-300/S7-400 Loadable CP Driver: MODBUS RTU, S7 is Slave SIMATIC S7-300/S7-400 Loadable CP Driver MODBUS RTU, S7 is Master S7 Open Modbus TCP I hope this helps |
Cheers |
|
This contribution was helpful to
3 thankful Users |
Follow us on