1/10/2017 3:45 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello, how many time the card has been used as far as I know no, then if you have a 32DI 6ES7 321-1BL00-0AA0 if I remember correctly there is no the successor because it would 6ES7 321-1BL01-0AA0. So to see an older card to another, or watch this number in the code or on the front panel there is also a E-Stand as shown below. The FAQ below is for panel but you will see also in your card. It is just for you if you want to see if it is older than another. How can you determine the "E-Stand" (hardware release) of an operator panel? |
Follow us on