8/20/2014 11:04 AM | |
Posts: 247 Rating: (2) |
Hello experts, I have to do programming for 7SR11 SIEMENS protection relays, i want to know is S7 300 or 400 PLC supportsIEC60870-5-103. |
8/20/2014 1:33 PM | |||
Joined: 9/27/2006 Last visit: 9/24/2024 Posts: 12282 Rating: (2685)
|
Hello Ravi; Standard S7-300 and S7-400 CPUs do not support IEC-60870-5 protocols natively. However Siemens provides so-called Siplus RIC bundles (including the CPU, MMC card, communication interface module and program blocks for the specific IEC 60870-5 variant you choose) that are dedicated to sub-station communications. See here (in the Siemens Industry Mall) for more details (RIC bundles are also available for the S7-400, look at the navigation tree at the left of the link page): SIPLUS RIC S7-300 bundles IEC 60870 - Industry Mall Overview If a SIMATIC S7-300 based system is to communicate with a Siemens control center, e.g. SIMATIC PCS 7 TeleControl, WinCC TeleControl, WinCC OA, or a control center of a third-party supplier using the IEC60870-5 telecontrol standard, the IEC 60870-5-101 (serial), -103 (protection) or -104 (TCP/IP) telecontrol protocols can be used in the SIMATIC automation systems. SIPLUS RIC bundles offer an integrated, scalable system based on SIMATICS7-300 functions, for the following data quantities: • 200 information points, with CPU314 • 1000 information points, with CPU315 • 2000 information points, with CPU317 • 5000 information points, with CPU319 The non-retain memory can now also be used for buffering message frames. Longer communication failure times can thus be bridged. The SIPLUS RIC software libraries are based on the standard SIMATIC Manager and can be used on various, mutually compatible types of SIMATIC S7 devices – this saves hardware costs and programming overhead. Example: Part number of the S7-315-2PN based RIC bundle for IEC 60870-5-103 protocol:
Finally, have a look at the following manual on the program blocks for IEC 60870-5-103: SIPLUS RIC IEC on S7 Functional description IEC 60870-5-103 Master Version V1.5 Hope this helps, Daniel Chartier |
||
Last edited by: dchartier at: 8/20/2014 1:46 PMLast edited by: dchartier at: 8/20/2014 1:36 PM |
|||
This contribution was helpful to1 thankful Users |
8/20/2014 1:55 PM | |
Posts: 1058 Rating: (93) |
Hello RaviS, there are bundles of S7 314 and SIPLUS RIC IEC60870-5-103 Master available. More details you will find here: SIPLUS RIC Bundles with S7-300 You might also be interested in this: SIPLUS RIC IEC on S7 Functional description IEC 60870-5-103 Master Version V1.5 SIPLUS RIC IEC on S7 Interoperability list IEC 60870-5-103 Master V1.5 regards |
8/20/2014 3:23 PM | |
Posts: 1058 Rating: (93) |
If you look in manual SIPLUS RIC IEC on S7 Functional description IEC 60870-5-103 Master Version V1.5 you will find following under chapter 4.1.2 - ASDU-Address Parameter-DB: In the parameter DB the ASDU addresses and the assignment to the corresponding device (link address) have to be indicated. The path for reaching the respective ASDU is defined via this assignment. System related, the maximum number of the link and ASDU addresses is only limited by the DB length. Up to 8 link and ASDU addresses have been tested. regards |
This contribution was helpful to1 thankful Users |
8/24/2014 10:46 PM | |
Joined: 9/1/2005 Last visit: 9/18/2024 Posts: 4104 Rating: (195) |
closed cause question published twice. The second thread with the subject Can the Siemens PLC support IEC60870-5-103is published within the conference Communication / Networks. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on