2/8/2017 8:02 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980) |
Hello, can you try to upload in HWConfig? Regards Christoph |
2/8/2017 8:12 AM | |
Joined: 4/28/2015 Last visit: 4/12/2024 Posts: 112 Rating: (3) |
Dear Sir, I have tried to upload in HW Config but still the same error. I have managed to get the backup of this project when i try to open the project it displays the below error. I have seen the vfd number and firmware from the back up project and installed the gsd in my software. |
Thanks |
|
2/8/2017 8:22 AM | |
Joined: 4/28/2015 Last visit: 4/12/2024 Posts: 112 Rating: (3) |
I have searched for PROTOOL software but seems it is discontinued and the replacement is WINCC FLEXIBLE 2008 sp2 which i am currently downloading and installing. But is the PROTOOL the actual problem for the g120 not appaering in the hardware configuration. |
Last edited by: Satheesh290692 at: 2/8/2017 8:26:33 AMThanks |
|
2/8/2017 8:23 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980) |
Hi, this message means that the project contains a ProTool HMI Device and the SW is not installed on the system. And which VFD with which FW?
Christoph |
2/8/2017 8:48 AM | |
Joined: 4/28/2015 Last visit: 4/12/2024 Posts: 112 Rating: (3) |
Dear Sir, How can I find whether the software is installed in Starter OM ? I have attached the details of the g120 drive below. |
Thanks |
|
2/8/2017 9:07 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980) |
Hi, if you can see the drives and open the properties then the correct OM is installed on the System.
Christoph |
2/8/2017 10:39 AM | |
Joined: 4/28/2015 Last visit: 4/12/2024 Posts: 112 Rating: (3) |
any other solution experts? |
Thanks |
|
Follow us on