12/17/2014 11:59 AM | |
Joined: 10/3/2013 Last visit: 10/26/2023 Posts: 123 Rating: (3) |
Dear All, I have also some doubt regarding memory concept of S7-300 & S7-400. In CPU S7-300 is working with memory card & without battery then why it is not reset/cleared from work memory or initialize from memory card when power not available. While, In CPU-S7 400, if there is no batteries then it is reset/cleared from work memory orinitialize from flash cardwhen power not available. Reagards, Mahesh N
|
Last edited by: Min_Moderator at: 12/18/2014 9:41 AMSplitted |
|
12/18/2014 11:01 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello Have you already seen this: How can you obtain an overview of the memory concept of SIMATIC S7-300 CPUs and C7 devices? How can I get an overview of the S7-400 memory concept? |
This contribution was helpful to1 thankful Users |