5/7/2019 2:49 PM | |
Joined: 5/22/2015 Last visit: 4/11/2024 Posts: 118 Rating: (2) |
Hi, I need to established communication between Robot Comau (Master) and S7-300 Slave. It's possible to connect him ? |
5/7/2019 3:01 PM | |
Joined: 5/22/2015 Last visit: 4/11/2024 Posts: 118 Rating: (2) |
I want to use Profibus communication. My PLC is 313c-2dp |
5/7/2019 3:06 PM | |
Joined: 9/27/2006 Last visit: 4/24/2024 Posts: 12257 Rating: (2665)
|
Hello Mohamed; Searching on the Comau site brings up no information on Profibus, either master or slave. What robot do you plan on using, what Profibus master communication card is in your design? What is the Profibus configuration software for this master? If you already have a Profibus master for your robot and the Profibus configuration software to configure it, then all you should need is the gsd file for the S7-300 CPU. You can select your specific CPU's gsd file in this link: Profibus gsd files: Simatic https://support.industry.siemens.com/cs/ww/en/view/113652 You must integrate this gsd file in the Profibus configuration software you will use, then insert an instance of your S7-300 in the slave list, and design the data exchange modules required for communication with the master. Since we have no detailed information, this is a very general answer. We can perhaps be more informative if you provide more details on your system. Hope this helps, |
This contribution was helpful to3 thankful Users |
Follow us on