9/28/2015 4:18 PM | |
Joined: 1/28/2009 Last visit: 4/26/2024 Posts: 6836 Rating:
|
Hello, yesterday again there was a power failure and again the original hardware configuration was restored and the same fault was there what should i do to prevent the CPU from reverting back to its previous configuration?? is it the faulty batteries that are causing this problem or should i copy RAM to ROM after downloading the modified configuration. If you are external flash memories, you need to download the final user program to that,You can find the procedure in the following FAQ.In addition, you need to replace the old batteries by checking the indications on PS or lack of sufficient power (losing internal RAM data of CPU in case of a power failure): How can I get an overview of the S7-400 memory concept?
hdhosseini |
This contribution was helpful to
1 thankful Users |
8/2/2016 7:31 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating:
|
New question published by nkr is split to a separate thread with the subject Error when I try to open hardware configuration. Best regards |
8/30/2016 3:31 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating:
|
New question published by AutoGen_148962 is split to a separate thread with the subject Redundant CPU and redundant IM in a non redundant configuration. Best regards |
Follow us on