8/26/2019 4:03 PM | |
Joined: 4/7/2015 Last visit: 6/18/2024 Posts: 27 Rating: (2) |
Hello, Vishakha! Do you have additional information about your problem? diagnostic buffer,hardware and netpro configurations,error values from modbus blocks?? Follow to this manual to configure MODBUS TCP communication in H-systems: SIMATIC SIMATIC Modbus/TCP Redundant communication via the CP 443-1 in H-systems |
Last edited by: valrin at: 08/26/2019 16:07:51Last edited by: valrin at: 08/26/2019 16:08:36 |
|
This contribution was helpful to1 thankful Users |
8/27/2019 8:27 AM | |
Posts: 3093 Rating: (323)
|
Hello, Regards, |
8/27/2019 2:31 PM | |
Joined: 2/8/2018 Last visit: 3/28/2023 Posts: 256 Rating: (4) |
Hello Sir, Thanks for the reply. Well I am trying Single redundant client function. CP 443-1 2qty's , CP1 - IP Address : 192.168.0.3 Remote Port : 502 CP2 - IP Address : 192.168.0.4 Remote Port : 503 Now when I give ENQ command to true then i get status as "A0FF" for one CP which means connection is not ready , and another CP status is 16#000 + Busy - 0 amd Error also 0 , done too 0 and no data transfer. Can anyone suggest what might be the problem. Values for all parameters are correct as per given in the manual. |
Last edited by: Vishakha at: 08/27/2019 14:32:42 |
|
8/27/2019 6:31 PM | |
Posts: 3093 Rating: (323)
|
1. install the hotffix Regards, |
8/29/2019 2:34 PM | |
Joined: 2/8/2018 Last visit: 3/28/2023 Posts: 256 Rating: (4) |
Ok sir, will try thanks |
Follow us on