11/30/2017 2:52 PM | |
Joined: 7/27/2015 Last visit: 3/27/2024 Posts: 109 Rating: (2) |
Dear All, I am using s7 400 PLC. PLC is not coming to run mode. showing following error. Module Information - CPU 412-2 PN "Diagnostic Buffer" Tab Event 1 of 120: Event ID 16# 5371Distributed I/Os: End of the synchronization with a DP master/IO controller on slot 2Number of distributed stations: 23No relevance for user: 24Incoming event06:05:16.496 PM 11/30/2017(Coding: 16# 5371 2402 C450 0017 0024 0000) Event 2 of 120: Event ID 16# 530DNew startup information in STOP modeStartup prevented by:- STOP request exists- Cold restart or warm restart necessaryStartup information:- Time for time stamp at the last backed up power on- Single processor operationCurrent/last startup type:- Automatic warm restart after backed up power onPermissibility of certain startup types:- Manual warm restart permittedLast valid operation or setting of automatic startup type at power on:- No startup type/following memory resetOperating mode: STOP (internal)Incoming event06:04:11.484 PM 11/30/2017(Coding: 16# 530D FF04 C777 0041 0810 0700) Please find the attachment Attachmentdi.pdf (285 Downloads) |
Follow us on