8/25/2009 10:01 PM | |
Posts: 58 Rating: (1) |
Hi Niranjan, It seems to be a hardware problem. Have you set up the 2 racks as rack 1 and 2? (Switch at the back of the CPU) |
8/26/2009 10:26 AM | |
Posts: 691 Rating: (37) |
Dear Maha, i am attaching the Screen Shot of Diagnostic Buffer as you have requested in the previous Thread. Please Find it And I have done proper rack settings int the two H-CPUs Thanx for Replying this Thread AttachmentDiagnose.zip (469 Downloads) |
Last edited by: Niranjan at: 8/26/2009 10:30 AMLast edited by: Niranjan at: 8/26/2009 10:28 AM |
|
This contribution was helpful to1 thankful Users |
8/26/2009 4:09 PM | |
Posts: 118 Rating: (4) |
Hi, 1.Have u done the above steps mentioned (Delete system file and compile again)and downloded the HW configuration to each cpu. 2.While downloading have u received any warning popup mentioned like infollowing link /tf/WW/en/Posts/12651 because the diagnostic buffer fault is look like same above link. 3.Is it your Interface Submodule having any difference with the actual configured one. |
Last edited by: Maha at: 8/26/2009 4:11 PM |
|
This contribution was helpful to1 thankful Users |
9/1/2009 12:55 PM | |
Posts: 86 Rating: (7) |
http://support.automation.siemens.com/NL/view/en/34894744 Hi. In this entry you find information about replacing the CP card. It look like there are differences between the older and newer firmware of old cp I think it is a must to go to the newer CP card becauce the ---1ex11-- is going out. Yer |
Follow us on