4/28/2012 12:44 PM | |
Posts: 559 Rating: (87) |
Dear All, Sorry for my mistake that I wrote to communicate HMI on Y-Link. It is only possible way to use Repeaters only. |
4/28/2012 2:49 PM | |
Joined: 12/1/2009 Last visit: 9/5/2024 Posts: 672 Rating: (147) |
No problem SolutionFinder, I do mistakes as well and try my best to learn from them. But it's a nice ideato have a devicelikea Y-LINK which works with HMI's as well, rather using thisrepeater stuff. I hopeR&D people are reading this post as well. Regards. |
Give us your feedback and show us your respect! |
|
4/28/2012 3:08 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (272) |
Hello, Let me disagree with you in this regards because of two reasons. Reason1: The cost of Y-LINK with ET200M bundle will more then Repeater cost. Isn't it? Reason2: When you do not connect any device on Y-LINK, you cannot download the hardware to CPU. In case let us you configured Hmi on Y-LINK and if Hmi got damage then in such case you will get SF On CPU and on ET200M as well Which will not be the Case in Repeaters |
Last edited by: Amit_86 at: 4/28/2012 4:48 PMLast edited by: Amit_86 at: 4/28/2012 4:46 PMVANDE MATARAM..... |
|
4/28/2012 3:12 PM | |
Joined: 12/1/2009 Last visit: 9/5/2024 Posts: 672 Rating: (147) |
Dear Amit_86, sorry, but you did not read or understood my post. Regards. |
Give us your feedback and show us your respect! |
|
6/6/2012 8:38 AM | ||||
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hello Komaruddin, Here is the Document for you.... I don't know why they have removed this good Document..... Attachment23842653_WinCC_flexible_redundant_communication_e.pdf (312 Downloads) |
|||
Ammy |
||||
6/6/2012 8:48 AM | |
Posts: 4 Rating: (0) |
Hi Ammy, Many thanks for the document... It's very usefull for me. Rgds, Komaruddin
|
6/11/2012 6:51 AM | |
Posts: 94 Rating: (8) |
Dear Amit, TIBI68 said a device like Y-link which will work with HMIs, not the Y-link... but its Nice idea... to have a device like that |
Follow us on