3/23/2017 1:11 PM | |
Joined: 10/13/2011 Last visit: 2/6/2019 Posts: 12 Rating:
|
Hello Just to be sure, that you have a suitable License-paper. You should find the following strings which you need for further tasks: - DESIGO S7 BACnet-Integration Runtime-License for 1 CPU Start the Web License manager .... .. and use the entry: "Direct access with barcode" even if you do not have a bar code. 1. Select product: "S7BACnet DESIGO" 3. Enter your license Nr. e.g. T-A3QS07103 ... 5. Generate license key 6. Enter this License key and the dispatch note number in the Mapping-tool where you define the mapping between S7-DB-Variables and BACnet objects. If you have any difficulties regarding this device, please create a Support-request. Good luck! |
This contribution was helpful to
2 thankful Users |
3/27/2017 1:48 PM | |
Joined: 10/13/2011 Last visit: 2/6/2019 Posts: 12 Rating:
|
Hello Well it's really interesting, I got same request, same time, also from Italy, from Filippo Tirini. I asked him to generate a Support Request. He did it and I provided him the necessary SW and documentation. May be you work on the same project, then please ask Filippo Tirini, otherwise please create also a support request: Have a nice time |
Follow us on