5/1/2019 9:26 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (818)
|
Hello, thnx for picture. In this case that CPU is really next generation, you can also use EM277 (if you have) with DP Profile configured on WinCC side (KTP cfg). Speed can be configured from 187.5 in my opinion or set only max allowed by PLC via MicroWin->System Block but your PLC type need to be recognized already. Use simply recommended DP cable with DP plugs/connectors for interconnection PLCand HMI. About MPI connection it need to be again tested, it can work in my opinion but maybe due lower firmware only PPI or DP profile can be set. I think that cfg with TIA Portal will be without problems. |
Last edited by: Duris_I at: 05/01/2019 09:28:01Last edited by: Duris_I at: 05/01/2019 09:35:18With best regards... |
|
Follow us on