5/10/2017 7:27 AM | |
Posts: 144 Rating: (7) |
Hello S7-300-315 2DP Wincc 6.0 I have a problem with S7-Graph FB and its instances.When using multiple instances for the FB it works fine but when i use "Check consistency " and compile the block i get the error " Only one instances can be generated automatically..." . In this Link as i understand, it says that there must be only one instance per S7-Graph FB!! .In other word to reuse the FB you should create another FB and assign another DB to it.right? The point is besides the error in compiling ,the FB works OK with multiple instances. I want a clear description of the solution. Thanks for your help. |
Last edited by: r.ethernet at: 5/10/2017 7:29:17 AM |
|
5/15/2017 9:55 AM | |
Joined: 11/27/2015 Last visit: 9/11/2024 Posts: 7 Rating: (0) |
Hi. Im also looking for this answer. so hopefylle someone is answaring :)
|
Follow us on