7/7/2009 5:03 PM | |
Joined: 9/28/2005 Last visit: 8/27/2024 Posts: 2957 Rating: (242) |
Hello, I have had something similar to your problem. My problem was if I open one HMI (the project has several of them) everything is ok. Then I close it and try to open another one from the same project then I get crash. Solve to my problem was like this: 1. Open one HMI and work 2. Close this HMI 3. End task of HmiES.exe 4. Open next HMI and have no problem As long as reboot of computer don't help that there might be some other problem or this problem is because you do not end task HmiES.exe before opening another one. By the way, you can download and install SP1 for Flexible 2008 from here http://support.automation.siemens.com/WW/view/en/34778772 and then you can have HF1 for this newly installed SP1 from here http://support.automation.siemens.com/WW/view/en/36540041 |
Last edited by: Darius at: 7/7/2009 5:06 PMBest regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on