12/18/2019 5:10 AM | |
Joined: 4/18/2014 Last visit: 5/3/2024 Posts: 253 Rating: (5) |
Hi experts , My PLC is S71200 and my CPU is 1214C and am communicating the Datalogic barcode scanner by rs232 configuration via ET200sp Modules (CM PtP(Freeport, 3964R, USS, Modbus RTU) ===> 6ES7137-6AA00-0BA0). I want sample program for the same. i found lot of links but none of them is fully solved , so if you have sample program please share the same. Because programming is same for any brand of bar code scanner if the protocol is same right. Regards, Attachmentdatasheet_quickscaniqbt2400.pdf (890 Downloads) |
Last edited by: GUWS at: 12/18/2019 05:34:04Last edited by: GUWS at: 12/18/2019 08:40:50 |
|
12/18/2019 11:47 AM | |
Joined: 9/9/2014 Last visit: 3/26/2024 Posts: 242 Rating: (40) |
Hello, I think that everything is quite simple, because standard instructions are used for data exchange via RS232. Unfortunately, I do not have an example program for exchanging data with a scanner, but after reading the topics below, it’s not so complicated ("DATALOGIC" scaner have their own examples and good manuals, so you can figure it out quickly) FAQs Connecting a Scanner / Barcode Reader to the Integrated PtP Interface on the CPU S7-31xC Topics: S7-1200, how to get a data from a barcode reader S7-1200 connecting to Barcode reader How can I read data from a barcode scanner to a S7-1200? Siemens SI ASCII Card (RS232C) with a barcode scanner Sample program for barcode scanner Communication with barcode reader RS232 Communication With ET200S SI Module CM 1241 RS232 communication with Motorola LS2208 barcode scanner connect s7-1200 to 17 barcode scanner Read the topics, at the initial stage they will definitely help))) |
Last edited by: Jen_Moderator at: 12/18/2019 14:47:10Optimized link. Best Regards |
|
This contribution was helpful to1 thankful Users |
12/19/2019 8:21 PM | |
Joined: 9/9/2014 Last visit: 3/26/2024 Posts: 242 Rating: (40) |
Hello, Found what you need (on our forum) - especially for you. Look at the topics below - they will definitely help, especially the first one (thanksDenilson Pegaia) First: Sample program S7-1200 RS 232 ASCII HyperTerminal comunications Second: Siemens S7-1200 and RS232 communication... getting started with RS232 (CM1241) s7-1200 and rs232 tutorial request! If this helps, and you have no more questions - please close the topic and rate) Thanks in advance! |
Last edited by: Unreality at: 12/19/2019 20:21:41Best Regards |
|
12/20/2019 12:45 PM | |
Joined: 9/9/2014 Last visit: 3/26/2024 Posts: 242 Rating: (40) |
Especially for you GUWS Look at the topic (I added a project there with PLC firmware 4.2 and TIA PORTAL 15.1): Sample program S7-1200 RS 232 ASCII HyperTerminal comunications |
Best Regards |
|
12/23/2019 1:51 AM | |
Joined: 4/18/2014 Last visit: 5/3/2024 Posts: 253 Rating: (5) |
Thank you Mr.Unreality , i will look on to this and update u |
Follow us on