9/2/2008 2:12 PM | |||||||||||||||||
Posts: 487 Rating: (44) |
There are two options. Both options will have as SM/CP/FMs are only allowed fromslot 4-11 as explained above. And what option to pick will depend on what CPU you have. If you have a CPU with built-in DP or PNinterface, the I will pick ET200M expansion rack with IM153-2 https://mall.automation.siemens.com/DE/guest/bizLogic/bizGotoMLFB.asp?nodeID=5000002&mlfb=6ES7153%2D2BA02%2D0XB0&siteID=DE&lang=en If you do not have DP interface, I will suggest to use with the IM 360/361. IM360 will sit on main rack IM361 is the connected to expansion rack
|
||||||||||||||||
Last edited by: JMJ at: 9/2/2008 2:25 PM |
|||||||||||||||||
Follow us on