6/6/2017 12:23 PM | |
Joined: 11/28/2016 Last visit: 9/5/2024 Posts: 1 Rating: (0) |
Dear All, Greetings!!! Please find attach Architecture, Details CPU-315-2PN/DP, ET-200M,(Red Bundle) CP-342-2 No's I want to achieve software redundancy with CP please let me know if possible or not. AttachmentSYSTEM ARCHITECTURE M-520.pdf (238 Downloads) |
6/7/2017 9:05 AM | |
Joined: 1/2/2014 Last visit: 8/16/2024 Posts: 142 Rating: (22) |
Hello, I guess your configuration is wrong and should change the CP selected. Please find the below Pdf and in page 62 it's clearly mentioned what all modules can be used. Also since configuration already used one CPU- MPI/DP port for ET200 staitons, where the DCS profibus connecting to? Additionally, active bus modules (6ES7195-7HB00-0XA0 or 6ES7195-7HC00-0XA0) for all the IO cards in ET200 station is a must for 300 based redundancy solution. For HMI to be connected automatically on redundancy switch over HMI must be triggered based on events/scripting. But for the DCS data, I doubt how data should be accessed at DCS end after detecting the switchover. AttachmentMAIN PDF SWR.pdf (217 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on