7/28/2006 8:35 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315)
|
Hi, For Fetch and Write you have to built up the header to do this... [:o] You can find this in the handbook where the 16 bytes of the frame are described. Structure of WRITE Frames The meaning and values of parameters shown without values in the following table can be found in the section “Parameter Values“ Structure of FETCH Frames The meaning and values of parameters shown without values in the following table can be found in the section “Parameter Values“. E. Linking to Other Systems with FETCH/WRITE So after this you know what you have to do with other scada-packages.. [:mad:] |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on