7/9/2015 12:55 PM | |
Joined: 1/28/2009 Last visit: 4/1/2024 Posts: 6836 Rating: (1359)
|
Hello, Despite the fact that an upload from the F/FH systems is possible, it is not helping.To migrate you need to the latest updates for STEP 7 V5.5 and accessing the offline project and 2 passwords.In this manner, it is possible to find out which version of F-system optional package is used to develop it.If you have the exact mentioned software, you change the hardware, compile and then compile the safety program and check if it produces the same signature as the original back up. A helpful manual can be found here to describe you which type of software components are required for working with F-System: SIMATIC Industrial Software S7 F/FH Systems - Configuring and Programming I hope this helps, hdhosseini |
Follow us on