(11)| 4/13/2018 4:54 AM | |
|
Posts: 1 Rating:
|
Hai Denilson, As i tried to open the Modbus TCP with S7-1500 TIA V14 but i can't open so please help me how to open that TIA V13 file on TIA V14 software. |
| 4/28/2018 3:38 PM | |
|
Joined: 9/23/2005 Last visit: 12/21/2025 Posts: 4433 Rating:
|
Hi, sorry but I don't have a V13 version of it. Anyway, Here there are a V15 version of a demonstration program and casts showing about how it was created. The project uses S7-1500 (but the configuration is similar to S7-1200). The use of S7-1500 has the advantage to be simulated in PLCSIM Advanced. The casts could be used as basis to build a project from zero. AttachmentMODBUS.zip (2863 Downloads) |
|
Denilson Pegaia |
|
This contribution was helpful to
|
|
| 8/7/2018 10:55 PM | |
|
Posts: 5 Rating:
|
Hi, with the internet examples, I made an example project between two s7-1200 (one as a server and the other as a client) maybe it can help you. use version 14 of the TIA PORTAL, CPUs with firmware version 4.2 and MODBUS instructions V4.1. The blocks were without optimized access. regards
AttachmentTestModbusClient_1_20180807_1549.zip (1554 Downloads) |
This contribution was helpful to
|
|
| 8/7/2018 11:00 PM | |
|
Posts: 5 Rating:
|
attachment video example... AttachmentModbus TCP S7-1200 Exe.zip (1383 Downloads) |
Last edited by: rojasalmut2 at: 8/7/2018 11:16:48 PM |
|
This contribution was helpful to
|
|
| 1/17/2019 10:59 AM | |
|
Joined: 12/8/2015 Last visit: 4/21/2021 Posts: 2 Rating:
|
Hi, Hope the attached program backup would help. |
This contribution was helpful to
|
|
Follow us on