5/12/2011 1:32 PM | |
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1425)
|
Hi, Note: the v13 SP1 / V14 versions of this project were publish in a post, here, at 27/sep/2017 AttachmentData Logging.zip (16129 Downloads) |
Last edited by: Pegaia at: 9/12/2011 12:26 PMAbout the sw version for the sample program Last edited by: Denilson Pegaia at: 9/27/2017 9:47:27 PMDenilson Pegaia |
|
This contribution was helpful to62 thankful Users
|
7/1/2011 3:33 PM | |
Posts: 4 Rating: (2) |
Thank you. Can Iask a question? -Where can change the file name of the datalog? (banana) . |
This contribution was helpful to1 thankful Users |
8/2/2011 1:00 PM | |
Joined: 8/21/2010 Last visit: 5/2/2024 Posts: 6 Rating: (1) |
Hello! How can I transfer the Logged data into 24 MB MMC? |
9/2/2011 10:23 PM | |
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1425)
|
Do you have SP1 or SP1 update1? |
Denilson Pegaia |
|
9/12/2011 2:41 PM | |
Posts: 7 Rating: (0) |
hi, i have STEP7 10.5 SP1 regards |
9/13/2011 12:49 PM | |
Posts: 25 Rating: (0) |
Impossible to open ? it's a zip-file, did you extractit ?? I was able to open it. My question ; I tried theexample on my home-PC & PLC and from the 1st try, I was ableto view the data log files. When I added the example to myreal program (other PC and PLC), I usedother markers and markerwords, but I suppose it's working because I see the nr Created increase when I do a DataLogCreate and the same when I do a DatLogWrite.So I suppose the logging is working. When I go to theinternet explorer, I get a datacommunication error instead of that screen of the S7-1200 CPU Webserver. My IP-addresses are 9.0.0.1 for the PC and 9.0.0.10 for the PLC and I enter http://9.0.0.10/ in my internet explorer. What is the problem here ??? If I close the file with a DataLogClose, it doesn't help. Is it necessary that the siemans-software is open and the a certain screen is activated or other preconditions ? Has it something to do with the IP-address starting with 9 instead of 10. Is it because it's another type of ethernet-port??? bart I found the answer (stupid) : enable the webserver in the properties of the configuration of the PLC |
Last edited by: BSALV at: 9/13/2011 3:04 PM |
|
1/16/2012 10:17 PM | |
Posts: 20 Rating: (1) |
I don't understand what i should do it. Can you explain more precisely. I'm doing everything it what was wrote in first post Pegaia |
1/19/2012 9:51 PM | |
Posts: 20 Rating: (1) |
Hello I'm attaching the watch table and a warnings what i have when I'm compile software. I'm doing everything the same what You are writing in first post. |
2/9/2012 11:51 AM | |
Posts: 23 Rating: (0) |
Hi, I have S7 1200 1212C with 2.12 firmware but I can`t use data logging. I don`t have SP1. Could that be the problem?
|
2/9/2012 2:29 PM | |
Posts: 23 Rating: (0) |
Thank you! I`m downloading the third part and I`ll try it when it`s done.
|
2/13/2012 7:51 AM | |
Joined: 8/31/2010 Last visit: 4/29/2024 Posts: 1509 Rating: (222) |
Hello HristoAtanasov , You can alternatively try to access the *.csv files using the S7-1200's integrated Web Server. Working with data logs in S7-1200so that you can confirm atleast if the data log is created. The complete details on DATA LOG instructions of S7-1200, Working with DATA LOG in S7-1200 is available here - DATA LOG in S7-1200 - Data Logging in S7-1200 |
Like it? Rate it! |
|
This contribution was helpful to1 thankful Users |
2/13/2012 10:53 AM | |
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1425)
|
Hi Polonez, Here there is a cast about my DATA LOG operation. I suggest you recompile HW and SW (all) before download it. I suggest you also reset to the factoring sets before the download. Attachmentoperating.zip (1959 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to1 thankful Users |
2/14/2012 4:35 AM | |
Joined: 8/31/2010 Last visit: 4/29/2024 Posts: 1509 Rating: (222) |
Hello HristoAtanasov, * Refer here to know on "How to set time of day using PG/PC?" * Here you find the instructions related to the Real Time Clock in S7-1200 - Date and time of day instructions |
Like it? Rate it! |
|
2/24/2012 11:25 AM | |
Posts: 6 Rating: (2) |
Hi Guys, is there a way to tell how full a datalog is? in other words I want to know before the log is full that it needs to be uploaded. |
2/25/2012 1:56 PM | |
Joined: 8/31/2010 Last visit: 4/29/2024 Posts: 1509 Rating: (222) |
Hello ok69a, Check here on Limits to the size of data log files in S7-1200 Make sure you don't exceed this in your application |
Like it? Rate it! |
|
4/16/2012 12:41 PM | |
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1425)
|
Hi, what is the command sequence that you are doing? |
Denilson Pegaia |
|
Follow us on