5/11/2012 9:35 AM | |
Posts: 2 Rating: (0) |
Hello guys, Does anyone have a success with Read/Write Sinamics' parameters via Profinet? I triedthis, butI can't make it working. Best regards |
5/23/2013 6:08 PM | |
Posts: 2 Rating: (0) |
Does anyone have a sample code or instructions for S7-1200 and Sinamics G120 with TIA v12 and Startdrive? |
5/24/2013 10:05 AM | |
Joined: 8/31/2010 Last visit: 3/27/2024 Posts: 1506 Rating: (221) |
Hello esbipa, You can have a look at the below URLs, which doesn't match your requirement 1:1 but this can help a little. SINAMICS G: Connecting of a G120 (Startdrive) using S7-300/400 (TIA-Portal) with PROFIBUS and HMI TIA Portal V12 Library with Faceplates for Controlling a SINAMICS G120 Drive with a SIMATIC S7-1200/300/400 Controller |
Like it? Rate it! |
|
7/25/2013 8:39 AM | |
Posts: 251 Rating: (11) |
can you connect s71200 with cu310? |
7/25/2013 9:54 AM | |
Joined: 8/31/2005 Last visit: 3/7/2024 Posts: 2197 Rating: (326) |
Yes, justimport the GSD or GSDML file of the CU310 in the TIA Portal and use Starter to parametrate the drive. In this FAQ you can see how to use a S120 with CU320 with the technological functions of the S7-1500. The CU310 can be used the same way. Even if you want to use control word and setpoint to control the drive (instead of the technological functions),you can find useful informations in this FAQ. |
|
|
This contribution was helpful to1 thankful Users |
9/26/2013 9:49 AM | |
Joined: 8/31/2005 Last visit: 3/7/2024 Posts: 2197 Rating: (326) |
Here it is: http://support.automation.siemens.com/WW/view/en/70155469 |
|
|
Follow us on