6/12/2014 11:18 AM | |
Posts: 67 Rating: (1) |
Hi All, I trying to make a single signal and monitor it by HMI i dont know what the wrong that i did. -First I defined an UDT with name "Pump" have run_cmd & RUNNGthen i make FC_FSD and write sample LAD one rung |/|----------(RUNNG) run_cmd also i insert the the FCs in the main OB and when i compile i didnt face any error (Perfect) :( -Second Add new divice and select my CPU .....etc >Roootscreeen I just add one text and the properites as the fig. [snip] ... and when i compile i have no error :( -thired I download the PLC blocks to PLCSIM and then Click on runtime for HMI screen then I changed the Value from PLC blocks (by change the run_cmd from close to open) but nothing happened in the HMI ...... Why :"( This the download link for my project for whom wanna show full program [snip] ... AttachmentD:\tmp\upload\AZRAIQI.zip (162 Downloads) |
Last edited by: CS Moderator at: 6/22/2014 3:52 PMProject as attachment |
|
6/14/2014 5:36 PM | |
Posts: 88 Rating: (12) |
Hello, Are you sure your communication between PLCSIMand WinCC Runtime is running good? This link could helpyouhttp://support.automation.siemens.com/WW/view/en/88193789 Regards, |
Follow us on