7/24/2007 7:50 AM | |
Posts: 19 Rating: (1) |
I have a problem at the moment. How do I write a single bit using the Sapi-S7 interface. I can't find an example anywhere :-( Yours sincerely /Jes |
7/24/2007 11:20 AM | |
Posts: 5822 Rating: (411)
|
Dear Jes, I am sorry but the last Samples for the SAPI S7 have been part of the Quick Start CD 4/2000. After this time the OPC Server has been used as the Standardinterface. I will add the PUT /GETSample for the PC side to this post... I hope it willhelp a bit, even so you will have to adapt the code anyway. Best regards J_Bell Attachments7_pc_300_tcp_v20.zip (405 Downloads) |
Follow us on