Industry Online Support
Technical Forum
6/1/2010 8:52 PM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Hello Svetoslav Veselinov, 1. When you are using memory card as "program card" then you load program into it. Internal memory of CPU is erased. Then the fully program (contains all of the code blocks and data blocks, any technology objects, and the device configuration) is on memory card and from there is execute. If you remove this card from CPU, there hasn't program. I don't know what is you idea, but is possible to keep some (limited 2048bytes) variables into CPU' retentive memory. The retentive memory area is used to store the values of selected user memory locations during power loss. When a power down occurs, the CPU has enough hold-up time to retain the values of a limited number of specified locations. These retentive values are then restored upon power up. 2. SIMATIC memory cards have a Windows file system and comply with the necessary industrial requirements. The memory card can be written to and read in any PC and then also used again for operation in the CPUs. Note:
3. Use SIMATIC S7 S7-1200 Programmable controller manual to understand how is possible to create different OB Hope this will helps. Best regards, Hristo Mihalev |
6/2/2010 12:54 PM | |
Posts: 21 Rating: (4) |
I'm very grateful, Hristo, thanks for your help. |
This contribution was helpful to1 thankful Users |
Follow us on