3/11/2014 3:13 PM | |
Posts: 1299 Rating: (136)
|
Hello, are there any error messages or log entries when you try to start logging? K!ke |
3/12/2014 11:33 PM | |
Joined: 1/14/2014 Last visit: 6/2/2024 Posts: 112 Rating: (1) |
Hi K!ke, thanks for the response. The shared settings are shown in the attached pictures. I'm attaching them as a zip file because I can't figure out how to attach multiple images at once. "Everyone" has full control and I am the owner. On the panel under Network ID I have only my name under "User name". No password, no domain. I didn't setup the panel to require a login yet. Is this a problem? Thanks for the help. AttachmentPermissions.zip (469 Downloads) |
3/13/2014 8:11 AM | |
Posts: 1299 Rating: (136)
|
Hello, see thisentry: http://support.automation.siemens.com/WW/view/en/13336639. There are all settings described. the settings you have to make on the panel are in chapter 1.2 K!ke |
Follow us on