10/23/2012 5:06 PM | |
Joined: 10/26/2011 Last visit: 9/9/2024 Posts: 762 Rating: (191)
|
The customer bought a 414-4H and has no money for the CP1613 and the redconect license? Unbelievable! I think, if you do it by your self, you won't have a real redundancy. You have to program so many things and you have to do so many tests. What do you do, if the customer is in manufacturing, one CPU is going in stop and the redundancy is not working? Then you have the liability, not Siemens. Additional, I think, that the attendance and maintenance of the programm is impossible. Also, your engineering costs willincreas up, and I promise, that they will be higher than the costs of the license and the CP 1613. One of so many questions: How do you do the synchronizing of the archives of the process data, the messages, alarms, warnings and so on I recomment, to buy the CP 1613 and the redconnect license! |
SIMATIC PCS 7 - Overview |
|
10/24/2012 1:47 AM | |
Joined: 9/19/2010 Last visit: 8/29/2023 Posts: 6 Rating: (0) |
Attached is the configuration file for your ref. Attachmentoverview.pdf (232 Downloads) |
Last edited by: O_Moderator at: 10/24/2012 7:56 AM |
|
10/24/2012 10:51 AM | |
Joined: 10/26/2011 Last visit: 9/9/2024 Posts: 762 Rating: (191)
|
Hello Dazhi, for the redundancy connection of a Touch Panel to a H-CPU, I find a very good application instruction. It is called "WinCC flexible redundant communication" http://support.automation.siemens.com/WW/view/en/43410086 On this page, you can also download Sample Scripts, which you can use for that. |
SIMATIC PCS 7 - Overview |
|
11/5/2012 5:55 AM | |
Joined: 9/19/2010 Last visit: 8/29/2023 Posts: 6 Rating: (0) |
Dear Thunderstorm/ Thanks for your valuable suggestion. |
11/5/2012 9:42 AM | |
Joined: 10/26/2011 Last visit: 9/9/2024 Posts: 762 Rating: (191)
|
You are welcome |
SIMATIC PCS 7 - Overview |
|
Follow us on