3/7/2008 11:33 AM | |
Posts: 5822 Rating: (411)
|
Hello, well i guess this is exactly your solution: Security with SIMATIC NET Best regards J_Bell |
3/7/2008 3:46 PM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating: (56) |
Hello, No at this way it's not possible. You always need to create Port Forwarding in the Router B in your case. This because certain traffic has to be directed towards de Scalance S612 in this case, and this traffic comes over ports 500/4500 UDP. Your example is described in the following faq: http://support.automation.siemens.com/WW/view/en/24953806 Furthermore it's also interesting to check or Router A is not blocking the ports 500/4500 because of an integrated Firewall. |
Best regards, |
|
10/31/2008 6:41 PM | |
Joined: 1/17/2006 Last visit: 5/1/2024 Posts: 552 Rating: (29) |
Hello, I'm having trouble to drag and drop both modules (module 1 - S612 andmodule 2 - SOFTNET Security Client) in one group (Group 1) as showed in FAQ. A message appears "This group only accepts modules in Routing-mode" (see attached file). What is my mistake ? Please for any help !! regards, Berg |
"Educate the children and it won't be necessary to punish the men." |
|
11/3/2008 2:52 PM | |
Joined: 1/17/2006 Last visit: 5/1/2024 Posts: 552 Rating: (29) |
Dear J_Bell, I'm sorry,I really had missed this part of the mentioned FAQ. My issue is about the Security Configuration Tool really.I've donethe stepsof the mentioned FAQ,and thegenerated file ".dat" isunknown for me. I have some doubts: 1) Could you tell me ifthe generated and editedcodeis correct ? 2) Thepart in bold of the showed belowcode has the IP addresses cleared, as follows: ip_address: 0.0.0.0 ip_mask as 0.0.0.0 What the reason of this behavior ? Maybe because the router A (like showed in FAQ) is a dynamicIP ? Thank you again ! regards, Berg ------------------------- <?xml version="1.0" encoding="utf-8"?> <SWSEM xmlns:xsd="http://www.w3.org/2001/XMLSchema" xmlns:xsi="http://www.w3.org/2001/XMLSchema-instance" xmlns="http://www.siemens.com"> <PC> <version>1.1</version> <name>Module2</name> <comment /> <def_router> <ip_address>0.0.0.0</ip_address> <ip_mask>0.0.0.0</ip_mask> </def_router> <router /> <pkcs12files> <pkcs12filename>Configuration1.MC1E2@G9A54.p12</pkcs12filename> </pkcs12files> <certificates> <certfilename>Configuration1.Group1.cer</certfilename> </certificates> </PC> <SEM> <name>Module1</name> <comment /> <ip_address>217.91.8.166</ip_address> <activelearn>no</activelearn> <secure> <group>2</group> <time>172800</time> <limit>0</limit> <encrypt1>3DES</encrypt1> <auth1>SHA</auth1> <encrypt2>3DES</encrypt2> <auth2>SHA</auth2> <pfs1>no</pfs1> <pfs2>no</pfs2> </secure> <ip_node /> <sub_node> <node> <ip_address>140.80.0.0</ip_address> <ip_mask>255.255.0.0</ip_mask> </node> </sub_node> <certfilename>Configuration1.Group1.cer</certfilename> </SEM> </SWSEM> ------------------------- |
"Educate the children and it won't be necessary to punish the men." |
|
Follow us on