5/20/2021 9:01 PM | |
Joined: 12/18/2014 Last visit: 9/18/2024 Posts: 33790 Rating: (4197)
|
In B006 you don't divide the value from analog amplifier trough 10, you add 10. |
5/20/2021 9:17 PM | |
Posts: 16 Rating: (0) |
i dont get it ! :-( i thought i am taking the result from the B002 and this i have to divide with 10 to get the right value. when it is 1000 it have to be 100 that is /10?? but yes it is not working when using /10 then the value is 32767 but when i use + 10 the 0 % value is 10 and the 100% value is 1010 Attachmenttemp 2.zip (230 Downloads) |
5/20/2021 9:27 PM | |
Joined: 12/18/2014 Last visit: 9/18/2024 Posts: 33790 Rating: (4197)
|
And with the correct settings you became the right results ... Attachmenttemp 2_V2.zip (211 Downloads) |
5/20/2021 9:31 PM | |
Posts: 16 Rating: (0) |
Please kick me :-) Rookie mistake. Like you said i was adding 10 i didnt get the "system" the + - / * under the value is of course for the line below not the line above :-( simple math it is working now here is the file Attachmenttemp 2.zip (224 Downloads) |
5/20/2021 9:32 PM | |
Posts: 16 Rating: (0) |
ahh you posted the file the same time i posted my answer :-) Thank you so much for your help Have a nice evening |
5/20/2021 9:45 PM | |
Posts: 16 Rating: (0) |
Properly a broken foot ;-) https://photos.app.goo.gl/6Mbz13sZG8AsbYbg7 |
Last edited by: ThomasGC at: 05/20/2021 21:47:15 |
|
Follow us on