8/13/2009 4:52 PM | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Joined: 1/17/2007 Last visit: 3/8/2024 Posts: 1541 Rating: (531) |
If I try to use breakpoints in the SCL editor, the editor crashes with an applications error. See the following screen dumps for the sequence of events that causes the crash (BreakpointCrash1 to 5). The system is S7-400 running id dual redundant mode. Software versions are:-
Any ideas what the problem is? AttachmentBreakpointCrash.zip (54 Downloads) |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Programming today is the race between software engineers building bigger and better idiot proof programs, and the universe producing bigger and better idiots. |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
8/13/2009 11:26 PM | |
Posts: 2661 Rating: (279)
|
This is a known problem (see page 4 of readme). Please upgrade SCL V5.3+SP1+HF4 to SP5: S7-SCL V5.3 + Service Pack 5 Released for Delivery Regards |
8/18/2009 10:14 PM | |
Posts: 2661 Rating: (279)
|
No, not when the system is in redundant mode. See attachment. AttachmentHOLD Mode.pdf (62 Downloads) |
Follow us on