7/10/2018 1:46 PM | |
Joined: 5/12/2006 Last visit: 9/23/2024 Posts: 22369 Rating: (3012) |
hello, do you get a error during the install? Christoph |
7/10/2018 1:51 PM | |
Joined: 3/14/2008 Last visit: 9/20/2024 Posts: 2095 Rating: (936)
|
Swagato, Which version of PCS7 are you working with? SCL comes with the supplied PCS7 Media DVD and is normally installed automatically. You should not install separate software from other sources than the Media DVD. PCS7 consists of several Siemens software programs such as Step7, CFC, WinCC and each software program has a specific version. When installing PCS7, you can choose a certain package like ES station or OS station. PCS7 installs the software automatically based on the chosen package. You should not install separate software programs by your own, only the ones which are released for PCS7. Are you sure PCS7 is installed on your system? When installed correctly, SCL is installed as well... |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
7/10/2018 2:57 PM | |
Posts: 29 Rating: (0) |
As far I remember I didnt get any error during installation
|
7/10/2018 7:15 PM | |
Joined: 3/14/2008 Last visit: 9/20/2024 Posts: 2095 Rating: (936)
|
Hi Swagato, Well, it could happen a block was protected (know how protection) , but it got unlocked and the source SCL is missing, then it could show you STL code. When a SCL code is compiled, it is translated to machine code, which is like STL. I think it also happens when you open the block in the Blocks folder, but the source is missing. The source is the SCL file which you can find under Sources in the S7 program folder. When you create your own block in SCL, you compile the source and a FB or FC is generated in the offline blocks folder. You then import the block in CFC if you want to use it. |
Last edited by: Oreca at: 7/10/2018 7:17:26 PMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
Follow us on