2/12/2010 8:00 PM | |
Joined: 12/25/2006 Last visit: 3/29/2022 Posts: 40 Rating: (1) |
Hi BerraB may be you can not see counting up because the counting too fast and the while function is ok and the block is rescan again... May be you can try ifinput or sometingthen index=0 end_if; this fonction end you can see what happend... the TimeTck is continuous from where it stopped.. |
automation and machine desing, project manager, drawing,programing, and automation responsable |
|
2/13/2010 10:28 AM | |
Joined: 1/29/2006 Last visit: 4/23/2024 Posts: 446 Rating: (64) |
Hey, BerraB ! To test, if your while loop is doing the job, I would simply return the value of your variable "Index", then I would concentrate on other statements in while loop..... for example: ..... the header and other stuff.... BEGIN Index:=0; END_FUNCTION |
Follow us on